Technical FAQs

Ask a Question

In the XVB Indicator Bank product line what amount of current draw does the DL1BDB LED bulb have on a 24VDC application?

Consumption LED unit
Steady 24 Vac/dc: < 80 mA
120 - 230 Vac: < 30 mA
Flashing 24 Vac or 24 Vdc: < 40 mA
120 - 230 Vac: < 15 mA
Unit with strobe (on energization) 24 Vac or 24 Vdc: 5 Joule unit: < 430 mA; 10 Joule unit: < 850 mA
120 Vac: 5 Joule unit: < 130 mA; 10 Joule unit: < 260 mA
230 Vac: 5 Joule unit: < 105 mA; 10 Joule unit: < 210 mA
Audible sounder units 12 - 48 Vac/dc: < 20 mA
120 - 230 Vac: < 50 mA


CTA-ID : 2022794
Was this helpful?
What can we do to improve the information ?