Technical FAQs

Ask a Question

Can the LA6DK10* mechanical latch block be mounted onto the Tesys series LC1D09 through LC1D38 or LC1DT20 through LC1DT40 contactors?

 Can old mechnical latch blocks be used with new Tesys D contactors?

Product Line:
 Tesys D contactors and accessories

Products sold and used in the United States
 Using old latch blocks with new contactors
No, the LA6DK10 is for use with the D1 and D2 series contactors only. Tesys series equivalent part number is LAD6K10*.

* - Complete part number with required control voltage suffix.
Note: this also applies to the reversing pairs LC2D09-LC2D38 and LC2DT20 through LC2DT40

CTA-ID : 2023367
Was this helpful?
What can we do to improve the information ?