Technical FAQs

Ask a Question

Does the Class L fuse bolt in a H367R switch?

Issue:
Application

Product Line:
HD SS

Cause:
Fuse mounting

Resolution:
Yes, the Class L fuse will bolt into the switch.


CTA-ID : 2023892
Was this helpful?
What can we do to improve the information ?