Technical FAQs

Ask a Question

What is the part number for a rectangular closing plate for the Class 8536 Type S NEMA 1 enclosed starter?

Issue:     
Identifying the part number for a closing plate for the knockout in a NEMA 1 enclosure

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Closing a knockout 

Resolution:
For slip on cover rectangular control station closing plate order 9999SG3.
For hinged door rectangular control station closing plate order 9999SG1.
For hinged door 30 mm round control station closing plate order 9001K51.
For slip on cover rectangular pilot light closing plate order 9999SG2.
For hinged door rectangular pilot light closing plate order 9999SG2.
For hinged door 30 mm round pilot closing plate order 9001K51.
For slip on cover rectangular reset operator closing plate order 9999SG2.
For hinged door 30 mm round reset closing plate order 9001K51.


CTA-ID : 2023412
Was this helpful?
What can we do to improve the information ?