Technical FAQs

Ask a Question

What is the part number for an auxiliary contact for 300, 400 600 and 800 amp Class 8903 Type S lighting contactor?

Select External Auxiliary Contact(s) from table below:

(1) normally open, field convertible 10 amp contact - 9999SX6
(1) normally closed, field convertible 10 amp contact - 9999SX7
(1) normally open, overlapping field convertible 10 amp contact - 9999SX9
(1) normally closed, overlapping field convertible 10 amp contact - 9999SX10
(1) normally open and (1) normally closed, isolated field convertible 10 amp contacts - 9999SX8

(1) normally open, non-field convertible 10 amp contact - 9999SX13
(1) normally closed, non-field convertible 10 amp contact - 9999SX14
(1) normally open, overlapping non-field convertible 10 amp contact - 9999SX15
(1) normally closed, overlapping non-field convertible 10 amp contact - 9999SX16
(1) normally open and (1) normally closed, isolated non-field convertible 10 amp contacts - 9999SX17



CTA-ID : 2023519
Was this helpful?
What can we do to improve the information ?