Technical FAQs

Ask a Question

Are replacement contacts available for the Class 8903 Type SQ NEMA 100 lighting contactor?

Yes, Class 9998 Type SL6 for two pole or Type SL7 for three pole devices.

If device is four or five pole it will be necessary to obtain two kits.

CTA-ID : 2023782
Was this helpful?
What can we do to improve the information ?