Technical FAQs

Ask a Question

Are Heavy Duty Safety Switches available with ANSI 61 paint instead of ANSI 49?

Issue:
Special options

Product Line:
Heavy Duty Safety Switch

Environment:
Special paint options

Cause:
Request for non-standard paint finish

Resolution:
Yes, but exceptions apply. Special paint options are not available for Type 4/4X/5 stainless steel, Type 4X fiberglass or Type 7/9 cast aluminum safety switches.
For Type 1, 3R, 12/3R or 12K switches, add suffix SP861 to the standard catalog number. A minimum purchase quantity of 10 is required.

CTA-ID : 2023474
Was this helpful?
What can we do to improve the information ?