Technical FAQs

Ask a Question

Are General Duty Safety Switches available with ANSI 61 paint instead of ANSI 49?

Issue:
Product options

Product Line:
General Duty Safety Switch

Enviroronment:
Special paint option

Cause:
Confirmation of special paint option

Resolution:
Special paint options are not available for the General Duty Safety Switch product line. For special paint options, please consider using Heavy Duty Safety Switches.


CTA-ID : 2023476
Was this helpful?
What can we do to improve the information ?