Technical FAQs

Ask a Question

Is the door for an MH-WP enclosure replaceable?

Issue:
Is the door for an MH-WP enclosure field replaceable?

Product Line:
Weatherproof Nema 3R/12 panelboard enclosures sold and supported in the USA.

Environment:
Maintenance

Cause:
Repair

Resolution: 
No this is not a replaceable part. The complete enclosure must be replaced.


CTA-ID : 2023482
Was this helpful?
What can we do to improve the information ?