Technical FAQs

Ask a Question

What is the significance of the second 9 on the LC*D099 or the 9 on the LC*D129?<br />What does the second 9 indicate on a LC1D099G7.

Represents Faston or Quick connect terminals.


CTA-ID : 2024137
Was this helpful?
What can we do to improve the information ?