Technical FAQs

Ask a Question

What is the replacement for a 997326 ML breaker?

Product Line:
Circuit Breakers
Obsolete ML type

Environment:
Electrical Distribution Equipment

Resolution:
This is a 200a 3p breaker. 240v 22k, 480v 18k, 600v 14k.
Use a KAL36200 and an SK4516. For use only in ML panels built after 1/1/1962, 31``, 38`` or 46`` wide and 10 5/8`` deep.


CTA-ID : 2024196
Was this helpful?
What can we do to improve the information ?