Technical FAQs

Ask a Question

Can the LC2D 4 pole contactors be used in reversing applications?

Issue: 
Can the LC2D pairs with 4 poles be used in reversing applications? 

Product Line:
 Tesys D contactors

Environment:
Products sold and used in the United States
 
Cause:
 Using a 4 pole LC2D pair of contactors
 
Resolution:
 
No, these 4-pole 4-pole contactors are configured for changeover applications. The standard LC2D 3-pole 3-pole contactors are configured for reversing applications.




CTA-ID : 2023935
Was this helpful?
What can we do to improve the information ?