Technical FAQs

Ask a Question

Is there a padlock attachment for the rectangular Class 9999 Type SA2, Type SA10, Type SC2 or Type SC22 cover mounted control units?

Product Line:
 
NEMA Type S Contactor and Starter Accessories
 
Resolution:
 
No, there are no padlock attachments nor do these units have padlock provisions.


CTA-ID : 2024219
Was this helpful?
What can we do to improve the information ?