Technical FAQs

Ask a Question

What are the contact ratings of standard XB4/XB5 (ie. ZBE101 ) contact blocks?

Issue:
What are the contact ratings of  standard XB4/XB5  (ie.   ZBE101 ) contact blocks?

Product Line:
22mm Push Buttons

Environment:
XB4/XB5 22mm Push Buttons

Cause:
Confirm the contact ratings for an application.   
                                              
Resolution:                                                                 
The contacts are rated NEMA A600. The maximum AC voltage is 600VAC and the maximum thermal current is 10 amps. Break ratings however are 1.2a at 600v, 3a at 240v and 6a at 120v .They are also rated NEMA Q600. The maximum DC voltage is 600VDC and the maximum thermal current is 2.5 amps. Break ratings are .1a at 600vdc , .27a at 250vdc and .55a at 125vdc
Was this helpful?
What can we do to improve the information ?