Technical FAQs

Ask a Question

Page 7-13 of Digest 173 list IEC operating mechanism LG8, shaft kits NS46 & NS446 as well as NW4 & NW4B operating handles for use with the GJL circuit breakers. Are these available for purchase?

The NS46, NS446, NW4 or NW4B at this point are not available and it is not expected that these will be available prior to 2007. Suggest continuing to use the current offering of 9421LG8, NS16 or NS336 and NW3 or NW3B listed on page 7-13 of Digest 172.

CTA-ID : 2024473
Was this helpful?
What can we do to improve the information ?