Technical FAQs

Ask a Question

What kind of input devices are used for 3 wire control with a contactor?

Use momentary (or spring return ) types like standard start and stop push buttons in conjunction with a holding circuit contact.

CTA-ID : 2024117
Was this helpful?
What can we do to improve the information ?