Technical FAQs

Ask a Question

What is the AIR for JG breakers?

Product Line:
Circuit Breakers

For Powerpact J Frame Circuit Breakers, the JG version has the following AIR:
65 kA @ 240 Vac
35 kA @ 480 Vac
18 kA @ 600 Vac
Was this helpful?
What can we do to improve the information ?