Technical FAQs

Ask a Question

How do you order factory installed auxiliary contacts on Class 8910 Type DPA contactors?

Issue:
How do you order factory installed auxiliary contacts on Class 8910 Type DPA contactors?

Product Line:
definite purpose contactors

Environment:
Products sold and used in the United States

Cause:
Factory installed auxiliary contacts

Resolution:
It is no longer an option.  They must be field installed.
However, this is the meaning for the forms:

Form
X01 - (1) normally closed
X02 - (2) normally closed
X10 - (1) normally open
X11 - (1) normally open & (1) normally closed
X12 - (1) normally open & (2) normally closed
X20 - (2) normally open
X21 - (2) normally open & (1) normally closed
X22 - (2) normally open & (2) normally closed
X30 - (3) normally closed
X31 - (3) normally open & (1) normally closed
X40 - (4) normally open


CTA-ID : 2024294
Was this helpful?
What can we do to improve the information ?