Technical FAQs

Ask a Question

Are replacement contacts available for the Class 8536 Type SE NEMA size three starter?

Product Line:
NEMA COntactors are starters

Resolution:
Yes, Class 9998 Type SL6 for two pole or Type SL7 for three pole devices.

If device is four or five pole it will be necessary to obtain two kits.


CTA-ID : 2024735
Was this helpful?
What can we do to improve the information ?