Technical FAQs

Ask a Question

What type of material is the enclosure on the Class 8903 Night-Master combination lighting contactors made of?

Depends on the enclosure designation; If ``C`` then the enclosure is painted sheet steel, if ``H`` then the enclosure is 304 stainless steel.


CTA-ID : 2024360
Was this helpful?
What can we do to improve the information ?