Technical FAQs

Ask a Question

QO13040L200WG: What is the retaining kit for backfeeding a 2 pole QO main breaker?

Issue:
Selection

Product Line:
QO Load Center Accessory

Environment:
Retaining kit selection

Cause:
Select correct accessory

Resolution:
If the back-fed breaker is 125A, or less, use PK4MB2HA. If the back-fed breaker is 150A - 200A, use PK5RK.


CTA-ID : 2025026
Was this helpful?
What can we do to improve the information ?