Technical FAQs

Ask a Question

Given the obsolescence of the NEHB panel, what is our solution for EHB-EPD functionality in an NF panel?

Issue:
Given the obsolescence of the NEHB panel, what is our solution for EHB-EPD functionality in an NF panel?

Product Line:
NF Panelboards and EDB, EGB and EJB breakers

Environment:
All NF Panelboards and only single pole EDB-EPD, EGB-EPD and EJB-EPD breakers

Cause:
What breakers can be used for equipment protection in NF Panelboards?

Resolution:
EDB-EPD, EGB-EPD and EJB-EPD circuit breakers are available in 15A, 20A, 30A, 40A and 50A configurations for use in NF panelboards. This design provides 30 milliampere ground fault pick-up levels per UL1053 at 277 Vac maximum. These circuit breakers are designed to protect equipment from ground fault damage. Each single pole EPD breaker requires two mounting spaces in the panelboard.


CTA-ID : 2024641
Was this helpful?
What can we do to improve the information ?