Technical FAQs

Ask a Question

Can I get a lug that will accept (2) 3/0 wire for L frame breaker catalog number LC36400? This is smaller wire than the standard lug will accept.

Product Line:
Legacy Circuit Breakers

Electrical Distribution Equipment

The AL600LI35 lug will accept (2) #1 to 350 kcmil wire.

Instruction bulletin 48040-734-02:

CTA-ID : 2025090
Was this helpful?
What can we do to improve the information ?