Technical FAQs

Ask a Question

What auxiliary contacts are provided as standard on Class 8736 Type SA, SB, SC or SD NEMA size 00 through 2 reversing starters?

There is 1 normally closed (9999SX12) auxiliary contact located in the lower right hand corner of each contactor wired from the factory for electrical interlocking purposes. There is also a normally open (9999SX11) auxiliary contact located in the upper left hand corner of each contactor for holding (seal in) circuit purposes.


CTA-ID : 2025750
Was this helpful?
What can we do to improve the information ?