Technical FAQs

Ask a Question

Can the Class 9999 Type SX__ external auxiliary contacts be stacked?

Yes with limitations based on contactor used as follows:
For Size 0 through Size 2 no stacking is allowed.
For Size 3 through size 7 one additional auxiliary contact can be stacked on to any one of the 4 external auxiliary contacts.

CTA-ID : 2025649
Was this helpful?
What can we do to improve the information ?