Technical FAQs

Ask a Question

Can a CA4KN relay be used with an auxiliary contact block?

Issue:
Determine if a CA4KN relay be used with an auxiliary contact block?

Product Line:
TeSys K IEC Relays

Environment:
CA4KN Low Consumption Control Voltage Relays

Cause:
To clarify if an auxiliary contact block can be used on a CA4KN relay.

Resolution:
The KN relays with low consumption coil can only be used with two pole auxiliary contacts. The four pole auxiliary contacts cannot be used.
 
Was this helpful?
What can we do to improve the information ?