Technical FAQs

Ask a Question

Is surge suppression supplied with the DC controlled LP*K__ K-Line contactors?<br />

Suppression is supplied with the low consumption DC controlled devices but not with the standard DC controlled devices. Order product with a ``3`` (i.e. LP1K0910BD becomes LP1K0910BD3) added to the voltage code to obtain this obtain from the factory.

CTA-ID : 2025704
Was this helpful?
What can we do to improve the information ?