Technical FAQs

Ask a Question

Do we have a mechanical lug for an MA or MH frame circuit breaker that accommodates qty. (3) 600 kcmil conductors per phase?

Product Line:
Legacy Circuit Breakers

Electrical Distribution Equipment

No, we do not have anything that will accept qty (3) 600 kcmil conductors per phase.

The customer may want to consider using a power distribution block, into which they could bring their conductors on one side and then run rated cable to the breaker.

CTA-ID : 2025563
Was this helpful?
What can we do to improve the information ?