Technical FAQs

Ask a Question

Can pilot light kit number 9999SP28R be applied with a mechanically held, NEMA 1 enclosed, Type LX lighting contactor with no control power transformer?

No, this kit cannot be used, because the location in the enclosure cover for the pilot light would place it directly in front of the mechanical latch on the contactor. The enclosure is not deep enough to prevent physical interference between the mechanical latch and the pilot light module. Additionally, this is a cover mounted light and this is not a hinged enclosure.

CTA-ID : 2026234
Was this helpful?
What can we do to improve the information ?