Technical FAQs

Ask a Question

What is the short circuit rating of a MHL361000 breaker in an MA1000R circuit breaker enclosure?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Cause:
Clarifying short circuit current rating

Resolution:
This enclosure will be rated per below as stated on wiring diagram in device:
65K at 208V or 240V
50K at 480V
25K at 600V
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009. CONSIDER USING THE M OR P FRAME POWERPACT CIRCUIT BREAKER IN THE M800 OR P1200 SERIES OF ENCLOSURES.


CTA-ID : 2026519
Was this helpful?
What can we do to improve the information ?