Technical FAQs

Ask a Question

Can the Class 8538 Type SB_ combination starter be supplied without the starter?

Yes add factory modification Y188. Y188 = basic combination starter less the open starter. Power wiring from the disconnect means and starter mounting hardware will be included.


CTA-ID : 2026051
Was this helpful?
What can we do to improve the information ?