Technical FAQs

Ask a Question

Are lugs provided on a SU3040D400CN?

Issue:  
Can I use 3rd party lugs on the SU3040D400CN CSED device?  

Product line:  
Residential Combination Service Entrance Devices

Environment:  
Ring type all-in-one CSEDs devices

Resolution:  
Lugs are not provided with this CSED device.  This device is supplied with line and neutral lug landing pads for use with field installed compression or mechanical type lugs.  For mechanical lugs, use lug kit CMELK4.  This lug kit consists of four lugs, each lug capable of terminating (1) #2 AWG - 600 kcmil aluminum or copper conductor.  Only three of the four lugs provided in the CMELK4 kit will be used.  

Optional mechanical lugs listed on the device wiring diagram include: ILSCO TA-600-2N (#2 AWG - 600 kcmil aluminum or copper), ILSCO TA-800-2N (300 - 800 kcmil aluminum or copper, Anderson L1D2-350 (#6 AWG - 350 kcmil aluminum or copper) or Anderson L1D2-800 (300 - 800 kcmil aluminum or copper).  Optional Anderson Compression lugs: Anderson VHCL-600-12BN (250 - 600 kcmil copper) or Anderson VHCL-750-12BN (500 - 750 kcmil copper).
Was this helpful?
What can we do to improve the information ?