Technical FAQs

Ask a Question

What power poles can be field added to the Class 8903 Type L*1000 or 8903LX*1000 lighting contactor?<br />

Remove existing single-pole adders and install one each of 8903L3L and 8903L3R to convert to 12-pole contactor.

CTA-ID : 2026937
Was this helpful?
What can we do to improve the information ?