Technical FAQs

Ask a Question

What is the acceptable wire size range for the termination points on the Class 8903 Type SV__ lighting contactor?

Power wiring: One aluminum or copper conductor #6 to 350 MCM (kcmil).
Control wiring: #16 to #12 AWG.

CTA-ID : 13148
Was this helpful?
What can we do to improve the information ?