Technical FAQs

Ask a Question

What`s the description and catalog number for a replacement coil excitation control module for a 8502 / 8536 Type SHO, size 6, series B contactor or starter?

31123-514-50 , This kit includes the control module for Size 6, Series B, and Size 7 Series A contactors and starters.

The control module is used to develop the two DC voltages used by the DC coil to pick the armature up and to keep it sealed (closed).

Kit part number 31123-514-50 includes the control module and installation instruction sheet 30072-151-59

CTA-ID : 2026993
Was this helpful?
What can we do to improve the information ?