Technical FAQs

Ask a Question

Is there an AC1 or resistive amp rating for the Tesys LUB__ or LU2B__ U-Line starter?

Product Line:
Tesys U Line Combination Motor Starter

Current rating is AC3 inductive for motor loads.

CTA-ID : 2026849
Was this helpful?
What can we do to improve the information ?