Technical FAQs

Ask a Question

What is the difference between a EK10201 and EK10202.

Issue:
Product Features

Product Line:
Safety Switch Accessory

Cause:
Clarifying difference in features

Resolution:
The EK10201 Electrical Interlock Kit has one normally open (1 NO) and one normally closed (1 NC) contacts. The EK10202 Electrical Interlock Kit has 2 normally open (2 NO) and 2 normally closed (2 NC) contacts .



CTA-ID : 2026847
Was this helpful?
What can we do to improve the information ?