Technical FAQs

Ask a Question

What is the temperature rating of the lugs on a Powerpact Q frame breakers?

Issue:
Breaker lug temperature

Product Line:
Molded Case Breakers 

Environment:
Powerpact Q

Cause:
Installation

Resolution:
The temperature rating is 75 degrees C.


CTA-ID : 2026854
Was this helpful?
What can we do to improve the information ?