Technical FAQs

Ask a Question

What is the fault current rating on a DJM32400E20 installed in an EZMR or EZMK 400A branch unit?

Product Line:
EZM Metering

Electrical Distribution Equipment

The SCCR ratings are:

65,000 AIR @ 240/120 Vac, 3-Phase, 4-Wire DELTA maximum, or
100,000 AIR @ 208Y/120 Vac, 3-Phase, 4-Wire maximum.

CTA-ID : 2027520
Was this helpful?
What can we do to improve the information ?