Technical FAQs

Ask a Question

Where are the EDS files for the ATV58 Devicenet communication card?

Issue:
Where are the EDS files for the ATV58 Devicenet option card.

Product Line:
Altivar ATV58 with Devicenet option card

Environment:
Product versions 5.X and 3.X only

Cause:
EDS files for the Devicenet option card for the ATV58 drives.

Resolution:
You will need to find the product version of the drive before you install your EDS file.   Remove the keypad from the VFD and you will see a white sticker with a product version on it.
I have attached ATV58 EDS files for product version 3.X and 5.X

CTA-ID : 2027180

Was this helpful?
What can we do to improve the information ?