Technical FAQs

Ask a Question

Can the Powerpact H & J frame breakers be backfed (reverse-fed)?

Yes, except as noted. The Powerpact H & J frame breakers with interchangeable trip units, identified by catalog numbers ending with a "T", are marked with "LINE & LOAD" connections, and are NOT able to be backfed.


CTA-ID : 2027390
Was this helpful?
What can we do to improve the information ?