Technical FAQs

Ask a Question

What is the replacement enclosure for Class 2510 Type MBG, Type MCG, Type TBG or Type TCG manual starter?

Issue: What is the replacement enclosure for Class 2510 Type MBG, Type MCG, Type TBG or Type TCG manual starter?

Product Line: 2510 type M and T manual starters

Environment: Products sold and used in the United States

Cause:Replacement enclosure part number needed for 2510M or 2510T manual starter

Resolution: The complete replacement enclosure is a 9991MG1.


CTA-ID : 2027436
Was this helpful?
What can we do to improve the information ?