Technical FAQs

Ask a Question

What is the function of auxiliary and alarm switches for molded case circuit breakers?

Issue:
What is the difference between and aux contact, alarm switch and overcurrent trip switch in a circuit breaker?

Product line:  
Molded case circuit breakers

Environment:  
Powerpact B, H, J, L, M, P and R frame circuit breakers

Resolution:
Auxiliary (OF) switches open or close when the breaker changes from the open to closed or closed to open condition.  Type "a" contacts are open when the breaker is open and closed when the breaker is closed.  Type "b" contacts are open when the breaker is closed and closed when the breaker is open.  
SD or Alarm contacts change state only when the breaker trips (for any reason).  They work off the mechanism and when the mechanism trips, they operate.  The are reset when the mechanism is reset.  
SDE or Overcurrent Trip Switch contacts change state only when the breaker trips due to an overcurrent.  They are reset when the breaker is reset.
Was this helpful?
What can we do to improve the information ?