Technical FAQs

Ask a Question

What type of receptacles are provided in a PAK75CTG Servicepak Power Outlet Panel?

Issue:
Product design feature

Product Line:
Servicepak

Cause:
Clarifying type of receptacles provided

Resolution:
This device is provided with (1) NEMA 5-20R receptacle (20A, 125V, 2W and Grd), (1) ANSI #73.13 receptacle (30A, 125V, 2W and Grd) and (1) NEMA 14-50R receptacle (50A, 125/250V, 3W and Grd).


CTA-ID : 2028636
Was this helpful?
What can we do to improve the information ?