Technical FAQs

Ask a Question

Are the Class 8940 pump panels CSA approved?


Issue:
Are the Class 8940 pump panels CSA approved?

Product Line:
Class 8940 Pump Panels

Environment:
Motor Starters

Cause:
Product Characteristics

Resolution:
No. They only carry UL and CUL approval.
 
Was this helpful?
What can we do to improve the information ?