Technical FAQs

Ask a Question

Do we have a lug for the Powerpact P Frame I-Line breaker that will accept (3) 600 kcmil cable?

Issue:
What is the part number for a lug to accept 3 - 600KCMIL cable for the Powerpact P frame I-line constructed breaker?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
No, we do not have a lug that will accept (3) 600 kcmil for I-Line.
One alternative is to terminate the 600 kcmil cables in a terminal distribution block and come to the breaker with cable rated for the lugs.
Another option is to use the Powerpact R frame breaker, which will accept (4) 600 kcmil conductors per phase.
Was this helpful?
What can we do to improve the information ?