Technical FAQs

Ask a Question

Is there a lug to lug kit for the Class 9065 Type SP____ Motor Logic Plus overload relay?<br />

9999MLPL, includes (2) lug shrouds, (3) terminal bus bars and (6) copper lugs which will accept (1) 14 AWG to 1/0 copper conductor per phase.

CTA-ID : 2027907
Was this helpful?
What can we do to improve the information ?