Technical FAQs

Ask a Question

What is the temperature rating for the lugs on a UFP222R pullout?

The lugs are rated for use with conductors with a 60 degree C or a 75 degree C temperature rating.


CTA-ID : 2028420
Was this helpful?
What can we do to improve the information ?