Technical FAQs

Ask a Question

Do we have a lug for (2) 350 kcmil for an LA, LAL, LH, LHL, Q4 or Q4L breaker?

Issue:
Is there a lug for (2) 350 mcm cable for an LA, LH or Q4 I-Line breaker?

Product Line:  
Molded case circuit breakers

Environment:  
Legacy LA, LAL, LH, LHL, Q4, Q4L breakers

Cause:
Product features.

Resolution:
The only option we have is the compression lug kit VC400LA35.  Using this kit, you can land two 250-350 kcmil Al/Cu conductors.  This kit contains 2 lugs for one terminal.  

Was this helpful?
What can we do to improve the information ?