Technical FAQs

Ask a Question

Is the QO200TR rated for use in commercial applications?

The QO200TR would be suitable for use in any application that does not exceed the maximum amperage, voltage and short circuit current ratings of the device. It is restricted to use in NEMA 1 or NEMA 3R applications, however. For more severe NEMA environments, other equipment should be used.


CTA-ID : 2028474
Was this helpful?
What can we do to improve the information ?